Hardware requirements
Mini/micro USB cable
EVK-MIMXRT595 board
Personal Computer
Board settings
Prepare the Demo
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J40) on the board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the power manager test demo in the terminal window:
Power Manager Test.
Please select the desired power mode:
Press A to enter: Sleep
Press B to enter: Deep Sleep
Press C to enter: Deep Power Down
Press D to enter: Full Deep Power Down
Waiting for power mode select...
Next Loop
Please select the desired power mode:
Press A to enter: Sleep
Press B to enter: Deep Sleep
Press C to enter: Deep Power Down
Press D to enter: Full Deep Power Down
Waiting for power mode select...