This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • Micro USB cable

  • EVK-MIMXRT595 REV C1 board

  • Personal Computer

Board settings

Make sure resistors R691~R697 are removed and resistors R611~R620,R660,R661,R698 are populated.

Prepare the Demo

  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J40) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the log would be seen on the terminal like:

FATFS example to demonstrate how to use FATFS with MMC card.



Make file system......The time may be long if the card capacity is big.



Create directory......



Create a file in that directory......



List the file in that directory......

General file : F_1.DAT.



 Write/read file until encounters error......



Write to above created file.

Read from above created file.

Compare the read/write content.

The read/write content is consistent.



Input 'q' to quit read/write.

Input other char to read/write file again.