Hardware requirements
Mini/Micro USB cable
FRDM-K32L2A4S board
Voltmeter
Personal Computer
Board settings
To measure the DAC output, connect J4-11 to positive of Voltmeter
Prepare the Demo
Connect a USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
A multimeter may be used to measure the DAC output voltage.
Running the demo
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
DAC basic Example.
Please input a value (0 - 4095) to output with DAC: 200
Input value is 200
DAC out: 200
Then user can measure the DAC output pin to check responding voltage.