This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • Two Mini USB cable

  • FRDM-K32L2B board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo

  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board for downloading the program and supply power for the board, connect another USB cable between host PC and USB port on the target board.

  2. Download the program to the target board.

  3. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

  4. Open a serial terminal(like putty) to communicate with the board via virtual com.

Running the demo

The log below shows the output of this demo in the terminal window:

hello world.

Terminal will echo back the received characters.