Hardware requirements
Mini/micro USB cable
FRDM-K32L2B board
Personal Computer
Board settings
No special is needed.
Prepare the Demo
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Connect the analog signal source’s output to the input of used-defined comparator’s channel (defined as “DEMO_CMP_USER_CHANNEL” in source code.)
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
CMP interrupt Example
Then change CMP analog input, and watch the change of LED. - CMP0_IN0 (Jump J1-9) connected to VCC=3.3V (Jump J3-8): LED RED on - CMP0_IN0 (Jump J1-9) connected to GND (Jump J2-14): LED RED off