Hardware requirements
Mini/micro USB cable
FRDMK32L2B board
Personal Computer
Board settings
Connect input to J4-2
Prepare the Demo
Connect a USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
When the example runs successfully, you can see information from the terminal as below:
TPM input capture example
Once the input signal is received the input capture value is printed