This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • Mini/micro USB cable

  • FRDM-K32L3A6 board

  • Personal Computer

Board settings

This example project uses LPCMP instance 0(M4) or instance 1(M0) to compare the voltage signal input from channel 2(PTC9) with the voltage signal(half of VDDIO) output by LPCMP’s internal DAC and output different result. LED1 will turn ON/OFF corresponding to different result. So the voltage signal input from PTC9 should be changed to observe the dynamical LED state.

  • Input signal to J2-18

Prepare the Demo

  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the example.

Running the demo

The log below shows in the terminal window:

LPCMP Interrupt Example.