Hardware requirements
Micro USB cable
FRDM-K32L3A6 board
Personal Computer
USB to Com converter
Board settings
PTA25(J1-2) connect to TxD of the USB to Com converter. PTA26(J1-4) connect to RxD of the USB to Com converter. GND(J2-14) connect to GND of the USB to Com converter.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
7 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal(from USB To Serial Adapter):
Lpuart interrupt example with seven data bits
Board receives 8 characters then sends them out
Now please input: