Hardware requirements
Mini/micro USB cable
FRDM-K32L3A6 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the example in the terminal window:
XRDC example start
Set the peripheral not accessiable
Violent access at address: 0x40032000
The peripheral is accessiable now
Set the memory not accessiable
Violent access at address: 0x 8000000
The memory is accessiable now
XRDC example Success