This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • Mini USB cable

  • FRDM-KE02Z40M board

  • Personal Computer

Board settings

No special is needed.

Prepare the Demo

  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

I2C example – Read Accelerometer Value Found an MMA8451 on board , the device address is 0x1d . The accel values: status_reg = 0xff , x = 220 , y = 616 , z = 1946 status_reg = 0xff , x = 222 , y = 617 , z = 1937 status_reg = 0xff , x = 217 , y = 615 , z = 1941 status_reg = 0xff , x = 220 , y = 620 , z = 1941 status_reg = 0xff , x = 219 , y = 617 , z = 1933 status_reg = 0xff , x = 221 , y = 614 , z = 1933 status_reg = 0xff , x = 219 , y = 618 , z = 1933 status_reg = 0xff , x = 220 , y = 621 , z = 1936 status_reg = 0xff , x = 221 , y = 616 , z = 1939 status_reg = 0xff , x = 219 , y = 617 , z = 1945

End of I2C example .