This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • Mini/micro USB cable

  • FRDM-KE02Z40M board

  • Personal Computer

Board settings

ADC0_SE0 is ADC input channel and J2-2 is ADC input pin.

Prepare the Demo

  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the hello world demo in the terminal window:

ADC polling Example.
ADC Full Range: XXXX
Press any key to get user channel's ADC value.
ADC Value: 42
ADC Value: 17
ADC Value: 18
ADC Value: 15
ADC Value: 19
ADC Value: 15
...

The user can sample voltage by J2-2 pin.