Hardware requirements
Mini USB cable
Two FRDM-KE02Z40M boards
Personal Computer
Board settings
SPI board to board: Transfers data through SPI interface. SPI0 pins of the master board are connected to the SPI0 pins of the slave board.
MASTER BOARD CONNECTS TO SLAVE BOARD
Pin Name Board Location Pin Name Board Location
MISO J9 pin 5 MISO J9 pin 5
MOSI J9 pin 3 MOSI J9 pin 3
SCK J9 pin 1 SCK J9 pin 1
PCS0 J9 pin 7 PCS0 J9 pin 7
GND J9 pin 14 GND J9 pin 14
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
Prepare the Demo
===============
1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
2. Open a serial terminal on PC for OpenSDA serial device with these settings:
- 115200 baud rate
- 8 data bits
- No parity
- One stop bit
- No flow control
3. Download the program to the target board.
4. Reset the SoC and run the project.
Running the demo
===============
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
SPI board to board interrupt slave example started!
SPI transfer finished!
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~