This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • Micro USB cable

  • FRDM-KE15Z board

  • Personal Computer

Board settings

This example project uses ACMP instance 0 to compare the voltage signal input from channel 0(J4-2) with the voltage signal(half of VDDA) output by ACMP’s internal DAC. Green LED will be turned ON/OFF corresponding to different comparison result.

Connect ACMP channel 0(J4-2) to external voltage generator to avoid floating voltage. The example serial port output may be frequent change otherwise.

Prepare the Demo

  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

  • 115200 baud rate

  • 8 data bits

  • No parity

  • One stop bit

  • No flow control

  1. Download the program to the target board.

  2. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

${ANCHOR}