This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • Micro USB cable

  • Two FRDM-KE15Z boards

  • Personal Computer

Board settings

LPI2C one board:

  • Transfer data from MASTER_BOARD to SLAVE_BOARD of LPI2C interface, LPI2C0 pins of MASTER_BOARD are connected with LPI2C0 pins of SLAVE_BOARD

MASTER_BOARD        CONNECTS TO         SLAVE_BOARD
Pin Name     Board Location     Pin Name     Board Location
LPI2C0_SCL   J4-12              LPI2C0_SCL   J4-12
LPI2C0_SDA   J4-10              LPI2C0_SDA   J4-10
GND          J3-14              GND          J3-14

Prepare the Demo

  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

  • 115200 baud rate

  • 8 data bits

  • No parity

  • One stop bit

  • No flow control

  1. Download the program to the target board.

  2. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

LPI2C board2board EDMA example -- Slave transfer.


End of LPI2C example .