This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • Micro USB cable

  • FRDM-KE17Z board

  • Personal Computer

Board settings

Make sure the FXOS8700CQ(U12) on the board is installed to run this demo. No special settings are required.

Prepare the Demo

  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

  • 115200 baud rate

  • 8 data bits

  • No parity

  • One stop bit

  • No flow control

  1. Download the program to the target board.

  2. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

LPI2C example -- Read Accelerometer Value

Found a FXOS8700 on board , the device address is 0x1C .

The accel values:

status_reg = 0xff , x =    60 , y =   -80 , z =  2094

status_reg = 0xff , x =    54 , y =   -73 , z =  2088

status_reg = 0xff , x =    54 , y =   -77 , z =  2096

status_reg = 0xff , x =    57 , y =   -79 , z =  2096

status_reg = 0xff , x =    57 , y =   -83 , z =  2089

status_reg = 0xff , x =    55 , y =   -78 , z =  2102

status_reg = 0xff , x =    56 , y =   -77 , z =  2097

status_reg = 0xff , x =    57 , y =   -77 , z =  2085

status_reg = 0xff , x =    59 , y =   -78 , z =  2094

status_reg = 0xff , x =    56 , y =   -79 , z =  2093

End of LPI2C example .