Hardware requirements
Micro USB cable
FRDM-KE17Z512 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the MCU-LINK USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the MCU-LINK terminal like:
ADC LOW POWER PERIPHERAL DEMO
The Low Power ADC project is designed to work with the Kinetis SDK.
1. Set your target board in a place where the temperature is constant.
2. Wait until two Led light turns on.
3. Increment or decrement the temperature to see the changes.
Wait two led on...
Enter any character to begin...
---> OK! Main process is running...!
Note:
when the temperature is raised: LED RED on, LED GREEN off.
when the temperature is reduced: LED GREEN on, LED RED off.