This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • Micro USB cable

  • FRDM-KE17Z512 board

  • Personal Computer

Board settings

This example project uses ADC12 instance 0 to sample and convert the voltage signal input from channel 0(PTE9). So the voltage signal input from PTE9(J2-19) should be changed to observe the dynamical conversion result.

Prepare the Demo

  1. Connect a USB cable between the PC host and the MCU-LINK USB port on the board.

  2. Open a serial terminal with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the example.

Running the demo

${ANCHOR}