This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • Micro USB cable

  • FRDM-KE17Z512 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo

  1. Connect a USB cable between the host PC and the MCU-LINK USB port on the target board.

  2. Open a serial terminal with the following settings:

  • 115200 baud rate

  • 8 data bits

  • No parity

  • One stop bit

  • No flow control

  1. Download the program to the target board.

  2. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

RTC example: set up time to wake up an alarm
Current date time: 2014-12-25 19:00:00
Please input the number of second to wait for alarm
The second must be positive value
Alarm will occur at: 2014-12-25 19:01:11

Alarm occurs !!!! Current date time: 2014-12-25 19:01:12
Please input the number of second to wait for alarm
The second must be positive value
...............................................
...............................................