Hardware requirements
Type-C USB cable
FRDM-MCXA153 board
Personal Computer
Board settings
P1_4(J1-2) connect to CTimer simple PWM.
Prepare the Demo
Connect a Type-C USB cable between the host PC and the MCU-Link port(J15) on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows example output of the CTimer simple PWM demo in the terminal window:
CTimer example to generate a PWM signal