This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • Type-C USB cable

  • FRDM-MCXA156 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo

  1. Connect a Type-C USB cable between the host PC and the MCU-Link USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the GLIKEY driver demo in the terminal window:

GLIKEY Peripheral Driver Example

*Success* GLIKEY is not locked

*Success* GLIKEY Sync Reset done

*Success* GLIKEY Start enable done

*Success* GLIKEY Continue enable Step 1 pass

*Success* GLIKEY Continue enable Step 2 pass

*Success* GLIKEY Continue enable Step 3 pass

*Success* GLIKEY Continue enable  Step 4 pass

*Success* GLIKEY Continue enable  Step 5 pass

*Success* GLIKEY Continue enable  Step 6 pass

*Success* GLIKEY Continue enable  Step 7 pass

*Success* GLIKEY Continue enable Step Enable pass

SUCCESS: Register on index 2 can be now written!

*Success* GLIKEY End of operation done

End of example