Hardware requirements
Type-C USB cable
FRDM-MCXA156 board
Personal Computer
Board settings
LPSPI:
MASTER(SPI0) connect to SLAVE(SPI1)
Pin Name Board Location Pin Name Board Location
SOUT J6-6 SIN J3-9
SIN J6-5 SOUT J3-11
SCK J6-4 SCK J3-7
PCS0 J6-3 PCS1 J3-5
Prepare the Demo
Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal on PC for MCU-Link serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, you can see the similar information from the terminal as below.
LPSPI functional interrupt example start.
This example use one lpspi instance as master and another as slave on one board.
Master uses interrupt way and slave uses interrupt way.
Note that some LPSPI instances interrupt is in INTMUX ,you should set the intmux when you porting this example accordingly
Please make sure you make the correct line connection. Basically, the connection is:
LPSPI_master -- LPSPI_slave
CLK -- CLK
PCS -- PCS
SOUT -- SIN
SIN -- SOUT
LPSPI transfer all data matched!
End of example.