Hardware requirements
Type-C USB cable
FRDM-MCXC041 board
Personal Computer
Board settings
No special board settings.
Prepare the Demo
Connect a Type-C USB cable between the PC host and the OpenSDA USB port on FRDM-MCXC041 board.
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo. For detailed instructions, see Getting Started with Software Development Kit for MCXC041.
Running the demo
When the demo runs successfully, the board’s LED will blink.