This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • Type-C USB cable

  • FRDM-MCXC041 board

  • Personal Computer

Board settings

SPI one board:

  • Transfer data from MASTER_BOARD to SLAVE_BOARD of SPI interface, SPI0 pins of MASTER_BOARD are connected with SPI1 pins of SLAVE_BOARD

           MASTER_BOARD    CONNECTS TO   SLAVE_BOARD
Pin Name   Board Location                Board Location
MOSI       J2-8                          J2-8
MISO       J2-10                         J2-10
SS         J2-6                          J2-6
CLK        J2-12                         J2-12
GND        J2-14                         J2-14

Prepare the Demo

  1. Connect a Type-C USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 9600 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

Running the demo

When the demo runs successfully, the log would be seen on the OpenSDA terminal like:

Master Start...

Succeed!