This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • USB-C cable

  • FRDM-MCXC242 board

  • Personal Computer

Board settings

No special board settings.

Prepare the Demo

  1. Connect a mini/micro USB cable between the PC host and the OpenSDA USB port on FRDM-MCXC242 board.

  2. Download the program to the target board.

  3. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo. For detailed instructions, see Getting Started with Software Development Kit for MCXC242.

Running the demo

When the demo runs successfully, the board’s LED will blink.