This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • Type-C USB cable

  • FRDM-MCXC444 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo

  1. Connect a type-c USB cable between the host PC and the MCU-Link USB port (J13) on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the following message is displayed in the terminal:

ADC16_DoAutoCalibration() Done.
ADC LOW POWER DEMO
 The Low Power ADC project is designed to work with the Tower System or in a stand alone setting
 1. Set your target board in a place where the temperature is constant.
 2. Wait until two Led light turns on.
 3. Increment or decrement the temperature to see the changes.
 Wait two led on...

 Enter any character to begin...

 ---> OK! Main process is running...!

Note:

  • when the temperature is above the average: LED RED on, LED GREEN off.

  • when the temperature is below the average: LED GREEN on, LED RED off.