This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • Type-C USB cable

  • FRDM-MCXC444 board

  • Personal Computer

Board settings

The flexio_spi_slave_interrupt_spi_master example is requires connecting between FlexIO pins with SPI pins The connection should be set as following: FLEXIO SPI1 PCS0 J4-1 J2-6 SCK J4-3 J2-12 MISO J2-10 J2-18 MOSI J2-8 J2-20

Prepare the Demo

  1. Connect a type-c USB cable between the host PC and the MCU-Link USB port (J13) on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the log would be seen on the terminal like:

SPI Master interrupt - FLEXIO SPI Slave interrupt example start.

This example use one spi instance as master and one flexio spi slave on one board.

Master and slave are both use interrupt way.

Please make sure you make the correct line connection. Basically, the connection is:

SPI_master -- FLEXIO_SPI_slave

   SCK      --    SCK

   PCS0     --    PCS0

   MOSI     --    MOSI

   MISO     --    MISO

This is FLEXIO SPI slave call back.

SPI master <-> FLEXIO SPI slave transfer all data matched!