This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Overview

The lpi2c_edma_b2b_transfer_slave example shows how to use lpi2c driver as slave to do board to board transfer with a EDMA master:

In this example, one lpi2c instance as slave and another lpi2c instance on the other board as master. Master sends a piece of data to slave, and receive a piece of data from slave. This example checks if the data received from slave is correct. LPI2C slave works as supporting board to help demonstrate master EDMA trasnfer, actually uses interrupt way.

Toolchain supported

  • IAR embedded Workbench 9.30.1

  • MCUXpresso 11.6.0

Hardware requirements

  • Type-C USB cable

  • FRDM-MCXN236 board

  • Personal Computer

Board settings

To make the example work, connections needed to be as follows: Jumper setting:

MASTER(LPI2C2)                connect to        SLAVE(LPI2C2)
Pin Name    Board Location                      Pin Name    Board Location
SCL         J5 pin 5                            SCL         J5 pin 5
SDA         J5 pin 6                            SDA         J5 pin 6
GND         J5 pin 8                            GND         J5 pin 8

Other jumpers keep default configuration.

Prepare the Demo

  1. Connect the type-c and mini USB cable between the PC host and the USB ports on the board.

  2. Open a serial terminal on PC for the serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The following lines are printed to the serial terminal when the demo program is executed.

LPI2C board2board EDMA example -- Slave transfer.

Slave received data :
0x 0  0x 1  0x 2  0x 3  0x 4  0x 5  0x 6  0x 7
0x 8  0x 9  0x a  0x b  0x c  0x d  0x e  0x f
0x10  0x11  0x12  0x13  0x14  0x15  0x16  0x17
0x18  0x19  0x1a  0x1b  0x1c  0x1d  0x1e  0x1f


End of LPI2C example .