This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • Type-C USB cable

  • FRDM-MCXN236 board

  • Personal Computer

  • 3.5” TFT LCD module by NXP (P/N PAR-LCD-S035) Rev.A

Board settings

Attach the LCD shield to the FRDM board.

Prepare the Demo

  1. Connect a micro USB cable between the PC host and the MCU-Link USB port (J10) on the board

  2. Build the project.

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

Running the demo

If this example runs correctly, the sample GUI is displayed.