Hardware requirements
Type-C USB cable
FRDM-MCXN947 board
Personal Computer
Board settings
Prepare the Demo
Connect a type-c USB cable between the PC host and the MCU-Link USB port (J17) on the board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, you can see the similar information from the terminal as below.
FLEXSPI example started!
Vendor ID: 0xef
Erasing Serial NOR over FlexSPI...
Erase data - successfully.
Program data - successfully.
Note: This example support two flash type: Winbond W25Q64 and MT MT35XU512
Define EXAMPLE_FLASH_TYPE=FLASH_W25Q64 for flash type W25Q64
Define EXAMPLE_FLASH_TYPE=FLASH_MT35XU512 for flash type MT35XU512