This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • Micro USB cable

  • FRDM-RW612 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo

  1. Connect a micro USB cable between the PC host and the MCU-Link USB port (J10) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

  1. The following lines are printed to the serial terminal when the demo program is executed.

PINT Pin interrupt example

PINT Pin Interrupt events are configured

Press corresponding switches to generate events

  1. This example configures “Pin Interrupt 0” to be invoked when SW2 switch is pressed by the user. The interrupt callback prints “PINT Pin Interrupt 0 event detected”.