This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • Micro USB cable

  • FRDM-RW612 board

  • Personal Computer

Board settings

Connect SPI master on board to SPI slave on other board.

    Master_board(SPI1)           Slave_board(SPI1)
Pin Name   Board Location     Pin Name   Board Location
MISO       J1 pin 4           MISO       J1 pin 4
MOSI       J1 pin 2           MOSI       J1 pin 2
SCK        J2 pin 12          SCK        J2 pin 12
PCS0       J2 pin 6           PCS0       J2 pin 6
GND        J3 pin 14          GND        J3 pin 14

Prepare the Demo

  1. Connect a micro USB cable between the PC host and the MCU-Link USB port (J10) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the log would be seen on the terminal like:

Slave is working....

Succeed!