Hardware requirements
Micro USB cable
IMX95LP4XEVK-15 board
J-Link Debug Probe
12V~20V power supply
MIPI DSI panel
Personal Computer
Board settings
For MIPI DSI panel(10802340), connect MINISAS DSI port J20 to panel. For MIPI2HDMI card(19201080), connect MINISAS DSI port J20 to card.
Prepare the Demo
Connect 12V power supply and J-Link Debug Probe to the board, switch SW5 to power on the board.
Connect a micro USB cable between the host PC and the J31 USB port on the cpu board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the example.
Tips: The APP_DISPLAY_EXTERNAL_CONVERTOR can be set as 1 when you are using MIPI2HDMI card(ADV7535) only.
In this function, the default port is MIPI DSI port. If you want to change panel, please change as below in dpu_example.h #define DPU_DI_MIPI 1 #define DPU_DI_LVDS 0 #define DPU_EXAMPLE_DI DPU_DI_MIPI #define MX8_DSI_OLED2 1 (for MIPI DSI panel) or #define MIPI2HDMI 1 (for ADV7535)
Running the demo
When the example runs successfully, you can see the rectangles and diamonds shown in the screen.