This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • Personal Computer

  • IMX95LP4XBB-15-REV-A EVK board

  • 12V~20V power supply

  • J-Link Debug Probe

  • Micro USB cable

Board settings

Use the jumper to connect the J25 1-2, 3-4, 5-6

Please note this application can’t support running with Linux BSP!

Prepare the Demo

  1. Connect the 12V~20V power supply and J-Link Debug Probe to the board, and switch SW4 to power on the board.

  2. Connect a micro USB cable between the host PC and the J31 USB port on the target board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Either re-power up your board or launch the debugger in your IDE to begin running the example.

Running the demo

When the example runs successfully, you will see similar information from the terminal shown below.

 ADC polling example.
 Please press any key to get the conversion result.
 The channel 0 ADC conversion data is 4084.
 The channel 1 ADC conversion data is 3740.
 The channel 2 ADC conversion data is 2049.
 Please press any key to get the conversion result.
 The channel 0 ADC conversion data is 4085.
 The channel 1 ADC conversion data is 3741.
 The channel 2 ADC conversion data is 2049.
 Please press any key to get the conversion result.
 The channel 0 ADC conversion data is 4084.
 The channel 1 ADC conversion data is 3739.
 The channel 2 ADC conversion data is 2049.