This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • Micro USB cable

  • IMX95LPD5-EVK board

  • JLink Plus

  • 12V~20V power supply

  • Personal Computer

Board settings

No special is needed.

Prepare the Demo

  1. Connect 12V~20V power supply and JLink Plus to the board, switch SW4 to power on the board

  2. Connect a micro USB cable between the host PC and the J31 USB port on the target board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Either re-power up your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, following information can be seen on the terminal:


==FlexCAN loopback functional example -- Start.==


Send message from MB8 to MB9

tx word0 = 0x11223344

tx word1 = 0x55667788


Receved message from MB9

rx word0 = 0x11223344

rx word1 = 0x55667788


==FlexCAN loopback functional example -- Finish.==