Hardware requirements
Personal Computer
IMX95LPD5BB-19-REV-A EVK board
12V~20V power supply
J-Link Debug Probe
Micro USB cable
Board settings
Use the jumper to connect the J20 1-2, 3-4, 5-6
Please note this application can’t support running with Linux BSP!
Prepare the Demo
Connect the 12V~20V power supply and J-Link Debug Probe to the board, and switch SW4 to power on the board.
Connect a micro USB cable between the host PC and the J31 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either re-power up your board or launch the debugger in your IDE to begin running the example.
Running the demo
When the example runs successfully, you will see similar information from the terminal shown below.
ADC selftest example.
The channel 0 ADC conversion data is 4079.
The channel 1 ADC conversion data is 3743.
The channel 2 ADC conversion data is 2048.
The channel 0 ADC conversion data is 4092.
The channel 1 ADC conversion data is 3742.
The channel 2 ADC conversion data is 2050.
The channel 0 ADC conversion data is 4092.
The channel 1 ADC conversion data is 3744.
The channel 2 ADC conversion data is 2051.
The channel 0 ADC conversion data is 4093.
The channel 1 ADC conversion data is 3741.
The channel 2 ADC conversion data is 2051.
The channel 0 ADC conversion data is 4091.
The channel 1 ADC conversion data is 3744.
The channel 2 ADC conversion data is 2049.
Self-test error occurred!
ADC self-test watchdog sequence error occurred.