Hardware requirements
Micro USB cable
IMX95VERDIN-EVK board
J-Link Debug Probe
12V~20V power supply
Personal Computer
Board settings
Connect input signal to J57-1 and J29-7(GND).
Prepare the Demo
Connect 12V~20V power supply and J-Link Debug Probe to the board, switch S6 to power on the board.
Connect a micro USB cable between the host PC and the J4 USB port on the cpu board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the example.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
TPM input capture example
Once the input signal is received the input capture value is printed
Capture value C(n)V=1f61