This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • Mini/micro USB cable

  • K32W148-EVK Board

  • Personal Computer

Board settings

This example project does not call for any special hardware configurations. Although not required, the recommendation is to leave the development board’s jumper settings and configurations in default state when running this example.

Prepare the Demo

  1. Connect a USB cable between the host PC and the EVK board J14.

  2. Download the program to the target board.

  3. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, you will detect voltage toggle on J4.P31 of the EBB MB board. If the EVK board is used then the green led will blink.