This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • Mini/micro USB cable

  • KW45B41Z-EVK Board

  • Personal Computer

Board settings

Prepare the Demo

  1. Connect a USB cable between the host PC and the EVK board J14.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The following lines are printed to the serial terminal when the demo program is executed.

TPM example to output combined complementary PWM signals on two channels

If an LED is connected to the TPM pin, you will see a change in LED brightness if you enter different values
If no LED is connected to the TPM pin, then probe the signal using an oscilloscope
Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value: