This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • Type-C USB cable

  • KW47-EVK Board

  • Personal Computer

Board settings

This Example project does not call for any special hardware configurations. Although not required, the recommendation is to leave the development board’s jumper settings and configurations in default state when running this example.

Prepare the Demo

  1. Connect a USB cable between the host PC and the EVK board J14.

  2. Open a serial terminal with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the example.

Running the demo

These instructions are displayed/shown on the terminal window:

PFlash Example Start

PFlash Information:

Program Flash block bass address:\t%d KB, Hex: (0x%x)

Program Flash block Size:\t%d KB, Hex: (0x%x)

Program Flash block Sector Size:\t%d KB, Hex: (0x%x)

Program Flash block count Size:\t%d

Total Program Flash Size:\t%d KB, Hex: (0x%x)

Successfully Erased Sector 0x%x -> 0x%x

Program a buffer to a sector of flash:

Successfully Programmed and Verified Location 0x%x -> 0x%x
~~~~~~~~~~~~~~~~~~~~~~~
And you will find the flash hase been programed.