This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • Micro USB cable

  • LPCXpresso51U68 board

  • Personal Computer

Board settings

Populate jumper JP3. Connect SPI slave on board to SPI master on other board

Slave - SPI3
Pin Name   Board Location
MISO       J4 pin 3
MOSI       J4 pin 2
SCK        J4 pin 4
PCS2       J4 pin 7

Prepare the Demo

  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J7) on the board

  2. Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

Running the demo

When the demo runs successfully, the log would be seen on the CMSIS DAP terminal like:

This is slave example for SPI half-duplex interrupt transfer.

Slave is working....

The received data are:
  0x00  0x01  0x02  0x03  0x04  0x05  0x06  0x07  0x08  0x09  0x0A  0x0B  0x0C  0x0D  0x0E  0x0F
  0x10  0x11  0x12  0x13  0x14  0x15  0x16  0x17  0x18  0x19  0x1A  0x1B  0x1C  0x1D  0x1E  0x1F
  0x20  0x21  0x22  0x23  0x24  0x25  0x26  0x27  0x28  0x29  0x2A  0x2B  0x2C  0x2D  0x2E  0x2F
  0x30  0x31  0x32  0x33  0x34  0x35  0x36  0x37  0x38  0x39  0x3A  0x3B  0x3C  0x3D  0x3E  0x3F

Slave transfer completed.