Hardware requirements
Micro USB cable
LPCXpresso51U68 board
Personal Computer
Board settings
No special is needed.
Prepare the Demo
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J6) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo
When the demo runs successfully, the log would be seen on the CMSIS DAP terminal like:
USART RX ring buffer example
Send back received data
Echo every 8 bytes