Hardware requirements
Micro USB cable
LPCXpresso54628 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a micro USB cable between the host PC and the LPC-Link USB port (J8) on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows example output of the eeprom example in the terminal window:
EEPROM example begins...
Page 0 program finished!
Page 1 program finished!
Page 2 program finished!
Page 3 program finished!
Page 4 program finished!
Page 5 program finished!
Page 6 program finished!
Page 7 program finished!
Page 8 program finished!
Page 9 program finished!
...
Page 126 program finished!
All data is correct! EEPROM example succeed!