Hardware requirements
Micro USB cable
LPCLPCXpresso54628 board
Personal Computer
Jumper wire
Board settings
No special settings are required.
Prepare the Demo
Connect a micro USB cable between the host PC and the LPC-Link USB port (J8) on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Running the demo
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Start EMC SDRAM access example.
SDRAM Write Start, Start Address 0xa0000000, Data Length 2097152 !
SDRAM Write finished!
SDRAM Read/Check Start, Start Address 0xa0000000, Data Length 2097152 !
SDRAM Write Data and Read Data Succeed.
SDRAM Example End.