Hardware requirements
Micro USB cable
LPCXpresso55S28 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Note: MCUXpresso IDE project default debug console is semihost
Connect a micro USB cable between the host PC and the LPC-Link USB port (P6) on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the terminal like:
Usart interrupt example
Board receives 8 characters then sends them out
Now please input: