Hardware requirements
Mini/micro USB cable
LPCXpresso55S36 board
Personal Computer
Board settings
Prepare the Demo
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J1) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the following message is displayed in the terminal:
RTC Example START:
Start Time is 2015/1/21 18:55:30
Ring, ring, ring
Alarm Time is 2015/1/21 18:55:33
RTC Example END.
~~~~~~~~~~~~~~~~~~~~~~~