Hardware requirements
Mini/micro USB cable
LPCXpresso55S36 board
Personal Computer
Board settings
Prepare the Demo
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J1) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the hello world demo in the terminal window:
Press any key to start example.
Board will enter power deep sleep mode, and then wakeup by OS timer after about 5 seconds.
After Board wakeup, the OS timer will trigger the match interrupt about every 2 seconds.
Board wakeup from deep sleep mode.
OS timer match value reached
OS timer match value reached
OS timer match value reached