This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • 2x Mini/micro USB cable

  • LPCXpresso55S36 Development Board

  • Personal Computer

  • FreeMASTER 2.5 or later installed on PC

Board settings

No special settings are required. The demo communicates over a virtual serial line (CDC) interface implemented by the microcontroller application and available at the device USB port. Two USB cables are required, one for the debugger session and the other for the microcontroller device USB port connection Use J3 USB port.

Prepare the demo

  1. Connect a USB cable between the host PC and the Debug USB port on the target board.

  2. Compile and download the program to the target microcontroller.

  3. Run and resume application execution when debugger stops in the main() function.

Connect with FreeMASTER

  1. Connect the 2nd USB cable between host PC and the microcontroller USB port on the target board.

  2. Wait for the operating system to configure the new USB serial device and assigns the COMx port.

  3. Run FreeMASTER, use the Connection Wizard or open Project Options.

  4. Select serial communication, choose the newly installed COMx port and connect at speed 115200 bps.

  5. Start communication, FreeMASTER loads the initial TSA Active Content links in the Welcome page.

  6. Click the “FreeMASTER Demonstration Project (embedded in device)” in the Welcome page

  7. The demo is now running, you should be able to watch variable values and graphs.

More information

Read more information about FreeMASTER tool at http://www.nxp.com/freemaster. Feel free to ask questions and report issues at FreeMASTER’s community page at https://community.nxp.com/community/freemaster