This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • Mini/micro USB cable

  • LPCXpresso55S36 board

  • Personal Computer

Board settings

Prepare the Demo

  1. Connect a USB cable between the host PC and the MCU-Link USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the terminal will display similar information like the following:

mbedTLS version 2.26.0 fsys=150000000 Using following implementations: SHA: CSS PKC HW accelerated AES: CSS PKC HW accelerated AES GCM: CSS PKC HW accelerated DES: Software implementation Asymmetric cryptography: CSS PKC HW accelerated

MD5 : 4662.18 KB/s, 31.33 cycles/byte RIPEMD160 : 875.40 KB/s, 166.87 cycles/byte SHA-1 : 2350.95 KB/s, 62.11 cycles/byte SHA-256 : 41391.32 KB/s, 3.45 cycles/byte SHA-512 : 37291.83 KB/s, 3.83 cycles/byte ARC4 : 7274.51 KB/s, 20.04 cycles/byte 3DES : 380.14 KB/s, 386.25 cycles/byte DES : 995.42 KB/s, 147.21 cycles/byte 3DES-CMAC : 349.99 KB/s, 419.43 cycles/byte AES-CBC-128 : 32889.63 KB/s, 4.36 cycles/byte AES-CBC-192 : 29400.76 KB/s, 4.88 cycles/byte AES-CBC-256 : 26880.42 KB/s, 5.35 cycles/byte AES-XTS-128 : 1112.54 KB/s, 131.19 cycles/byte AES-XTS-256 : 1102.51 KB/s, 132.41 cycles/byte AES-GCM-128 : 9534.20 KB/s, 15.08 cycles/byte AES-GCM-192 : 9001.61 KB/s, 15.74 cycles/byte AES-GCM-256 : 8700.90 KB/s, 16.31 cycles/byte AES-CCM-128 : 4607.30 KB/s, 31.14 cycles/byte AES-CCM-256 : 4272.91 KB/s, 33.65 cycles/byte ChaCha20-Poly1305 : 932.59 KB/s, 156.78 cycles/byte AES-CMAC-128 : 4872.27 KB/s, 29.59 cycles/byte AES-CMAC-192 : 1098.19 KB/s, 133.17 cycles/byte AES-CMAC-256 : 4642.15 KB/s, 31.22 cycles/byte AES-CMAC-PRF-128 : 4820.65 KB/s, 29.90 cycles/byte CAMELLIA-CBC-128 : 1173.54 KB/s, 124.83 cycles/byte CAMELLIA-CBC-192 : 921.57 KB/s, 159.03 cycles/byte CAMELLIA-CBC-256 : 921.57 KB/s, 159.03 cycles/byte ChaCha20 : 1222.75 KB/s, 119.80 cycles/byte Poly1305 : 5063.30 KB/s, 28.84 cycles/byte BLOWFISH-CBC-128 : 1148.30 KB/s, 127.58 cycles/byte BLOWFISH-CBC-192 : 1148.30 KB/s, 127.58 cycles/byte BLOWFISH-CBC-256 : 1148.30 KB/s, 127.58 cycles/byte CTR_DRBG (NOPR) : 23935.43 KB/s, 6.03 cycles/byte HMAC_DRBG SHA-1 (NOPR) : 108.35 KB/s, 1363.20 cycles/byte HMAC_DRBG SHA-1 (PR) : 100.99 KB/s, 1464.84 cycles/byte HMAC_DRBG SHA-256 (NOPR) : 312.69 KB/s, 469.76 cycles/byte HMAC_DRBG SHA-256 (PR) : 312.68 KB/s, 469.76 cycles/byte RSA-1024 : 1754.00 public/s RSA-1024 : 105.67 private/s DHE-2048 : 0.33 handshake/s DH-2048 : 0.33 handshake/s ECDSA-brainpoolP512r1 : 21.33 sign/s ECDSA-secp384r1 : 41.67 sign/s ECDSA-brainpoolP384r1 : 42.33 sign/s ECDSA-secp256r1 : 98.00 sign/s ECDSA-secp256k1 : 98.33 sign/s ECDSA-brainpoolP256r1 : 100.00 sign/s ECDSA-secp224r1 : 111.67 sign/s ECDSA-secp224k1 : 111.67 sign/s ECDSA-secp192r1 : 166.67 sign/s ECDSA-secp192k1 : 167.00 sign/s ECDSA-brainpoolP512r1 : 13.33 verify/s ECDSA-secp384r1 : 21.33 verify/s ECDSA-brainpoolP384r1 : 21.67 verify/s ECDSA-secp256r1 : 64.33 verify/s ECDSA-secp256k1 : 63.67 verify/s ECDSA-brainpoolP256r1 : 65.33 verify/s ECDSA-secp224r1 : 61.00 verify/s ECDSA-secp224k1 : 60.33 verify/s ECDSA-secp192r1 : 94.00 verify/s ECDSA-secp192k1 : 94.33 verify/s ECDHE-brainpoolP512r1 : 11.00 handshake/s ECDHE-secp384r1 : 21.33 handshake/s ECDHE-brainpoolP384r1 : 22.00 handshake/s ECDHE-secp256r1 : 51.00 handshake/s ECDHE-secp256k1 : 51.00 handshake/s ECDHE-brainpoolP256r1 : 51.67 handshake/s ECDHE-secp224r1 : 58.00 handshake/s ECDHE-secp224k1 : 58.00 handshake/s ECDHE-secp192r1 : 87.00 handshake/s ECDHE-secp192k1 : 87.00 handshake/s ECDH-brainpoolP512r1 : 21.67 handshake/s ECDH-secp384r1 : 42.33 handshake/s ECDH-brainpoolP384r1 : 43.33 handshake/s ECDH-secp256r1 : 101.00 handshake/s ECDH-secp256k1 : 101.33 handshake/s ECDH-brainpoolP256r1 : 103.00 handshake/s ECDH-secp224r1 : 115.33 handshake/s ECDH-secp224k1 : 115.33 handshake/s ECDH-secp192r1 : 173.33 handshake/s ECDH-secp192k1 : 173.33 handshake/s