This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • Micro USB cable

  • LPCXpresso55s69 board

  • Personal Computer

Board settings

  1. Pin P19_2 is used as a CLKOUT signal. Connect this pin to an Oscilloscope for viewing the signal.

Running the demo

The demo sets the MicroTick Timer as a wake up source and puts the device in sleep mode. The MicroTick timer wakes up the device.

After wake up:

(1)the red LED on the board blinking. (2)CLKOUT signal changing can be seen on pin P19_2.And the frequency of output signal will double.

If the demo run successfully, you will see the log from debug console:

Utick wakeup demo start...
Wakeup from sleep mode...