Hardware requirements
Micro USB cable
Two LPCXpresso55s69 boards
Personal Computer
Board settings
Connect SPI master on board to SPI slave on other board
Master_board(SPI7) Slave_board(SPI7)
Pin Name Board Location Pin Name Board Location
MISO P17 pin 12 MISO P17 pin 12
MOSI P17 pin 10 MOSI P17 pin 10
SCK P17 pin 14 SCK P17 pin 14
SSEL1 P17 pin 1 SSEL1 P17 pin 1
GND P17 pin 7 GND P17 pin 7
Prepare the Demo
Note: MCUXpresso IDE project default debug console is semihost
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (P6) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo
When the demo runs successfully, the log would be seen on the CMSIS DAP terminal like:
Master Start...!
Succeed!
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~